Beyond inspecting individual parts, you'll want to ensure your equipment operates well as a whole. Here are our best tips for maintaining wheel loaders:
1. Refer to the Manual
Before beginning any kind of maintenance or work with a machine, you and your team should familiarize yourselves with each wheel loader's operation and maintenance manual. Equipment manufacturers provide documents with a wealth of useful information about settings, features, safety and maintenance.
Your wheel loader maintenance guide can tell you optimal fluid levels and change intervals, as well as cleaning and replacement intervals for filters. This manual will also tell you about each wheel loader's specific capabilities.
2. Inspect Attachments
Attachments make your wheel loader more versatile, and you want to make sure all the pieces are in top condition for years to come.
Different attachments call for different maintenance requirements, depending on what they do and how often you use them. Buckets are used for scooping and carrying materials, while forks are best for moving palletized loads across job sites. You can also use brooms for clearing debris from surfaces, rakes for land-clearing applications and couplers for quickly switching between attachments.
Inspect all your attachments before use, replace any problematic parts immediately, and store attachments properly when you don't need them.
3. Keep Equipment Clean
While making sure all your wheel loader's moving parts are operable is the first step to proper maintenance, keeping the equipment clean can also prevent some major issues. If possible, try to keep your equipment out of dirty conditions to begin with. However, if you do need to operate in mud and grime, proper cleaning is crucial.
Contaminants can build up on internal and external parts and lead to overheating and faster wear rates. Caked-on dirt can also hide small scratches and cracks that could turn into larger issues if left unchecked. Clean and inspect your equipment immediately after spending any time working in dirty conditions.
Especially in winter, where some areas experience freezing temperatures, you should always clear the mud from your wheel loader before putting it away at the end of a shift. Caked-on mud can freeze overnight and be difficult to remove the next time you need to use the machine. Follow the manufacturer's guidelines for cleaning more delicate parts, like chains and bearings.
4. Winterize
If you work in an area where wintertime means freezing temperatures, winterizing your heavy equipment is the best way to keep your fleet operable all year long. Preparing for dropping temperatures helps you maintain your investment.
Winterizing your equipment includes paying attention to:
- Fluids: Before winter, drain all your loader's fluids and replace them with products specifically made to withstand cold temperatures.
- Fuel: Tanks with low fuel can freeze overnight, so filling your fuel tank at the end of each shift ensures you have an easy startup the next morning.
- Batteries: Cold engines require more startup power, so keep your loader's batteries charged. If possible, you can remove them and store them indoors when not in use.
- Block heaters: Block heaters warm your equipment's engine and fluids before each shift, so startup is easy even in the cold.
- Warming equipment: Run your wheel loader for a few minutes before beginning operations to help it reach ideal temperatures and reduce wear.
5. Store Equipment Properly
At all times of the year, storing your equipment in the proper places can vastly increase its life span. In the winter, indoor storage is best if possible. Even a temporary shelter on a job site helps keep your machines out of the snow.
In the summer, a shaded storage area helps protect your equipment from harsh sunlight. Heat can damage many parts of your wheel loader over time, so using tarps, tents or other shade structures can make a significant difference.
6. Operate Properly and Safely
One of the best ways to maintain your wheel loader long into the future is to use it properly at all times. The recommended usage specifications listed in the operation manual or provided by your dealer are professional best practices. Wheel loaders come in different sizes with different amounts of power, various attachments and other key features.
Avoid using a wheel loader that's too small for a job or doesn't have the right features, as this can overtax the machine and lead to issues. However, a wheel loader that's too large may have trouble navigating tighter work sites. Your work site may also have equipment weight requirements you'll need to follow. Choose loaders that comply with site weight requirements.
Be mindful of bucket and load capacity as well. Only lift load weights and sizes your wheel loaders are built to carry to ensure attachments stay in good condition.
Overall, always making sure your equipment is best for the job and using it according to its specifications will help prevent avoidable mechanical issues.