Once you have identified a decrease in fuel pressure, the next step is to correct the issue and prevent future problems from occuring. Whether you plan to tackle repairs on your own or take your machine to a qualified mechanic, it's a good idea to check each of these critical areas of your machine so you can create an effective action plan:
- The gas tank: Start with your gas tank. Is it at least a quarter of the way full with quality, in-date fuel? Are there any visible signs of a leak, such as wet or sticky spots in the tank holding area?
- The fuel lines: If everything looks okay with your gas tank, it's time to check the nearby fuel line. Make sure it is connected and not broken, out of place or leaking fuel.
- The battery: If your fuel tank and lines are intact, the problem may be with your battery. Make sure all connections are hooked up between your battery and the rest of the machine system and test the life of your battery with a power probe or multimeter.
- The fuel pump: Next, locate and inspect your fuel pump, including the filter screen and relay element. If one or both of these parts is damaged, make the necessary replacements and try operating your machine as normal.
- The pressure regulator: Finally, if you identified no issues with the above elements, the problem is likely with the pressure regulator. Use a fuel pressure gauge to test your regulator. If you're not sure how to connect the pressure gauge, consult your owner's manual or local dealership. If the fuel pressure regulator is the problem, you will need to have it repaired or replaced by a professional.
If you have tried all of these steps to solve your fuel pressure problem, it's time to schedule an appointment with a qualified mechanic or equipment specialist so they can identify any more significant issues that may be at play.
Benefits of Fixing Low Fuel Pressure
If you have low fuel pressure, it's essential that you correct the problem sooner, rather than later. For you, fixing your machine's fuel pressure problem means:
- Efficient operation: Low fuel pressure can cause engine failure, difficulty accelerating and sluggish navigation. When you correct the problem, your machine becomes as efficient and easy-to-use as the day you first bought it. Stable pressure means you spend less time with a stalled machine and more time operating it.
- More resale value: If you plan to trade-in or resell your machine, it must first be in good working condition. Most dealerships and private owners are hesitant to accept a machine with visible issues — even if they are a simple fix — because there might be even more issues present that aren't as visible. Before advertising your machine for resale, make sure everything is operating as it should, and replace any faulty parts.
- Lower cost of operation: One of the biggest benefits of fixing low fuel pressure is how much you can reduce heavy equipment fuel costs. When equipment pressure is low, the system has to work twice as hard to try and correct the problem, and all that extra energy means you end up spending a lot more money on gasoline or diesel fuel. Additionally, if the pressure problem is a result of a leak, the extra fuel may end up in a puddle on the ground. By identifying and correcting the issue as soon as possible, you minimize the risk of wasting your money.
- Longevity: When something isn't working correctly inside your fuel pump, lines or engine, it puts pressure on other parts of your machine to operate more frequently or at a higher level than usual. Therefore, what begins as a simple problem with low fuel pressure can cause other parts to break down faster, resulting in a more costly fix in the future.
As you can see, fixing your fuel pressure problem is imperative to the efficiency and cost of operating your machine, as well as its overall value and longevity. However, fixing the problem is not enough — you should also take steps to prevent future pressure issues.
How to Stop Low Fuel Pressure and Prevent Future Issues
If you've gone through the work of locating, identifying and fixing the problem with your machine, the last thing you want is to run into a similar problem down the road. Here are some tips to reduce heavy equipment fuel pressure problems in the future:
- Change all filters regularly, including the filter screen and fuel filter.
- Use high-quality, in-date fuel from a trusted supplier.
- Rather than operate your machine at half-efficiency, perform diagnostic tests and replace all necessary parts as needed.
- Schedule maintenance check-ups throughout the year, so a mechanic can identify and correct possible concerns before they grow into larger ones.
By following these tips, you are doing your part to make sure your equipment and machinery operate efficiently for years to come.