We know taking the time to perform routine excavator maintenance is essential. It increases uptime, boosts your return on investment (ROI) and extends the life of your machine. On-site preventive maintenance procedures, in addition to scheduled check-ins at the shop, are key to gaining these benefits.
Here are some of the best excavator maintenance tips for minimizing wear and keeping your equipment in good condition.
1. Start With the Right Components
Choosing the best machine for the job may seem unrelated to maintenance, but it's crucial to maximizing your equipment's useful life. Along with performing the best work, the right machine will be able to withstand the demands of your operation longer than a machine that is suited for other applications could.
Purchasing a machine with components meant for other applications can cause unnecessary damage, which can lead to lost productivity and costly repairs.
For example, mismatching the machine's shoe width to your application can significantly accelerate undercarriage wear. The appropriate shoe width for your machine will depend on the machine's size and work environment — a wide shoe is best for soft terrain, while a narrower width is better for hard ground.
This rule goes for your fluids, too. You should always use an oil that meets the specifications in your O&MM, as choosing fluids that are too viscous — or not viscous enough — can harm your excavator's systems or cause power loss to friction.
2. Create and Follow an Efficient Management Program
The ideal equipment management program should include the following elements:
- Informed purchasing: Outlining a process for purchasing heavy equipment can help ensure you're choosing suitable machines for your operation. This process may include naming your preferred vendors and creating a list of all the features and benefits you're looking for. So when you go to purchase a new excavator, you're prepared.
- Scheduled maintenance: Sticking to an excavator maintenance schedule can help you minimize downtime and keep your machine working when you need it.
- Comprehensive operator training: Investing in both in-house and dealer training for your operators is crucial to maximizing your equipment's productivity and keeping your team safe. Properly trained operators will know how best to use a machine and what to look out for when issues arise.
- Fleet monitoring: A good fleet monitoring system can help you keep track of your equipment's maintenance history, parts purchasing and use, and upcoming scheduled procedures.
3. Use Excavators Properly
Before you put any machine on your work site, you should go over the use and maintenance guidelines in your O&MM.
Your operators should also familiarize themselves with this information before they can use the machine. A thorough training course can help ensure they understand the material and know the right procedures to follow.
Here are some excavator-specific operating tips:
- Make wide turns: Turning aggressively or pivoting the machine can speed up undercarriage wear and increase your chances of de-tracking.
- Dig toward idlers: Operators should always dig in the direction of the front idlers. Digging over the final drive or back toward the sprockets can cause structural damage to the undercarriage.
- Minimize time on slopes: If your operation requires digging on hills or other sloping terrains, it's best to get your excavators off the hill as soon as possible. Additionally, ensuring the drive motor is in the correct position — facing the back of the excavator — while working on slopes will reduce track wear.
4. Monitor Fluid Health
Fluids are the lifeblood of your machine. Performing a regular fluid analysis ensures vehicle health and improves your bottom line.
Key fluids to monitor include:
- Engine oil
- Hydraulic oil
- Gear oil for final drives
- Engine coolant
- Diesel fuel
You can perform these checks yourself, or, if your dealer offers this service, you can send fluid samples in to be tested at a professional lab.
Cat S•O•SSM Services provides professional fluid analysis from expert technicians to find signs of contamination, excessive wear or other hidden issues in the fluid samples you send in. You'll also get a full report of your machine's condition and actionable recommendations to bring your equipment back to full health. Talk to your local Cat dealer for more information.
5. Change Your Filters
Check your fluid and air filters frequently and replace them according to your O&MM's recommended intervals.
Engine air filters are important for keeping your engine free of dust, which can cause damage. Check this filter frequently to keep your engine dust-free. And make sure to avoid touching the secondary engine air filter during pre-shift checks.
Lastly, make sure to regularly clean out the cab's air filter. Your operators should always have clean air to breathe, after all.
Next-Gen Cat filters can reduce filtration costs by up to 15% with proper use and maintenance. Cat excavators group these filters together to allow for easy access.
Additionally, you'll want to keep an eye on your water separators. Cat machines have a sensor inside the cab to alert the operator when drainage is necessary, so you know it's time to clean it out if the light goes on.